• No : 21807
  • Release Date : 2018/08/22 16:29
  • Print

Frequency setting

I use the CC-Link option FR-A7NC to set the frequency to 60 Hz, but the monitor value is shown as "60.09 Hz" when the inverter operates.
Can I adjust it to 60 Hz?
Category : 

Answer

Since the Advanced magnetic flux vector control method uses slip compensation to compensate the frequency, the value is not shown as exactly 60 Hz.
For V/F control, check if slip compensation is enabled.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-A700