- No : 21894
- Release Date : 2018/08/22 16:29
- 
          
              Print
          
        
 
CC-Link, analog output card
    
      Can I use the CC-Link card (FR-A7NC E kit) and the analog output card (FR-A7AY E kit) simultaneously?  
    
  
    - Category : 
- 
      
    
 
    Answer
  
    You can install only one option card.
If you want to use two types of cards, replace the inverter with the FR-A700 series.
If you can use RS485 communication instead of CC-Link communication, you can connect a single analog output card to the standard PU connector port.
  
    
      
        - Product Name
- Inverter, magnet motor drive
        - Product Category
- Inverter
        - Series
- FR-E700