• No : 21908
  • Release Date : 2018/08/22 16:30
  • Print

Frequency setting

If I set up an external frequency setting potentiometer and connect to the terminals 10, 2, and 5, can I use this frequency setting potentiometer to command the reversible operation, forward and reverse rotations? 
Category : 

Answer

You can do so by setting Pr.73 to "10" or "11". (For A700/F700 (P), supply negative input to the terminal 1.)
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ