- No : 21962
- Release Date : 2018/08/22 16:30
-
Print
Using existing potentiometer by replacing inverter
When replacing existing inverters with the Mitsubishi products (for example, in facilities renewal construction), is it possible to use the speed varying potentiometers (1/2 W, 2 kΩ) used with the existing inverters with the new inverters?
The manual instructs to use 1/2 W, 1 kΩ. Is there any good method to do this?
- Category :
-
Answer
It is OK if the resistance value of the speed varying potentiometer's resistance is 2 kΩ.
Use the speed varying potentiometers used with the existing inverters as they are.
- Product Name
- Inverter, magnet motor drive
- Series
- Others