• No : 22055
  • Release Date : 2018/08/22 16:30
  • Print

Negative phase of input power supply

When the phase sequence of the input power supply to the inverter is reversed, how are the forward and reverse rotations of the inverter output influenced?
Category : 

Answer

The power supplied to the inverter is converted into DC by the converter inside the inverter and then stored in the capacitor. Thus, reversing the phase sequence does not influence the forward and reverse rotations.
Product Name
Inverter, magnet motor drive
Series
Others