- No : 22095
- Release Date : 2018/08/22 16:30
-
Print
Inverter installation interchange attachment
I am considering to upgrade from the FR-A200 series to the FR-A500 series (400 V, 3.7 kW).
The options column of the catalog indicates that the FR-A5AT03 applies to conventional types. Is this correct? (Can I upgrade from A200?)
- Category :
-
Answer
Use the FR-A5AT02 as the intercompatibility attachment when upgrading from the FR-A220-3.7K to FR-A540-3.7K.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A500