• No : 22095
  • Release Date : 2018/08/22 16:30
  • Print

Inverter installation interchange attachment

I am considering to upgrade from the FR-A200 series to the FR-A500 series (400 V, 3.7 kW).
The options column of the catalog indicates that the FR-A5AT03 applies to conventional types. Is this correct? (Can I upgrade from A200?)
Category : 

Answer

Use the FR-A5AT02 as the intercompatibility attachment when upgrading from the FR-A220-3.7K to FR-A540-3.7K.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A500