- No : 22131
- Release Date : 2018/08/27 16:41
-
Print
As to indication of the measurement value of the electric energy (EcoMonitorPlus/Light).
What happens when the measurement value of the electric energy exceeds 99999.9kWh(MWh)?
- Category :
-
Answer
It measures from 0kWh(MWh) after going round.
Integer 4 digits : 9999.98→9999.99→0000.00→0000.01kWh(MWh)
Integer 5 digits : 99999.8→99999.9→00000.0→00000.1kWh(MWh)
Integer 6 digits : 999998→999999→000000→000001kWh
- Product Name
- Energy Measuring Units
- Series
- EcoMonitor Plus, EcoMonitorLight