- No : 22133
- Release Date : 2018/08/27 16:41
-
Print
As to timing for outputting data file into the SD memory card.
When is the time to output data file from EMU4-LM into the SD memory card?
- Category :
-
Answer
EMU4-LM outputs data file at following timing.
1. When inserting the SD memory card while operating.
2. When power is ON in a state of the SD memory card inserted.
3. At every hour on the hour while operating in a state of the SD memory card inserted.
- Product Name
- Energy Measuring Units
- Series
- EcoMonitor Plus, EcoMonitorLight