• No : 22136
  • Release Date : 2018/08/27 16:41
  • Update : 2018/09/07 12:48
  • Print

As to logging period of the optional SD memory card (EMU4-SD2GB).

How long is the logging period of the optional SD memory card (EMU4-SD2GB).
Category : 

Answer

Logging period of the optional SD memory card (EMU4-SD2GB) is according to the logging cycle of detail data and the number of measuring circuits.

* It is the period until capacity of the 2GB SD memory card is exceeded during permanent connection. Data amount depends on the number of characters. It is the logging period where data is output at maximum volume.
Product Name
Energy Measuring Units
Series
EcoMonitor Plus, EcoMonitorLight