• No : 22155
  • Release Date : 2018/08/27 16:41
  • Update : 2020/04/10 16:04
  • Print

Measurable minimum load (ME96SS series).

What is the Measurable minimum load?
Category : 

Answer

In case of the input current of less than 0.005 A, the measurement values are as follows:
Current: 0 A,  Power supply: 0 W,  Reactive power: 0 var, Apparent power: 0 VA, and Power factor: 1.
Product Name
Electronic Multi-Measuring Instrument
Series
ME96SS series