• No : 22169
  • Release Date : 2018/08/27 16:41
  • Update : 2020/04/10 16:36
  • Print

Display upon upper/lower limit alarm (ME96SS series).

How does the screen change at the time of the upper/lower limit alarm?
Category : 

Answer

The measurement elements, including the digital indication, the unit indication and the phase indication, flash. And the “ALARM” indication and the “HI” indication or the “LO” indication flash.
In addition, it is possible to set the backlights to flash.
Product Name
Electronic Multi-Measuring Instrument
Series
ME96SS series