• No : 22175
  • Release Date : 2018/08/27 16:41
  • Update : 2020/04/10 16:51
  • Print

Disable an alarm for motor starting current (ME96SS series).

Is it possible to stop the alarm for motor starting current in the motor circuit?
Category : 

Answer

This model has “Motor Starting Current Mask Function”. This function stops the alarm output and updating of the maximum values during the setting time when a current value exceeds the threshold.
(Please refer to the Set-up menu 5 “Motor starting current delay time” of the section 3 in the User’s Manual.)
Product Name
Electronic Multi-Measuring Instrument
Series
ME96SS series