• No : 22254
  • Release Date : 2018/08/30 13:48
  • Print

Meanings of the sink input/source input

Answer

The sink input connects to a negative common for 24 V DC.
The source input connects to a positive common.

The sink input is generally used in Japan and North America.
The source input is generally used in Europe.
Product Name
FX1S, FX1N, FX1NC, FX2N, FX2NC, FX3S, FX3G, FX3GC, FX3U, FX3UC
Product Category
Main unit, I/O Extension
Series
MELSEC-F series