• No : 22263
  • Release Date : 2018/08/30 13:48
  • Print

Input wiring (FX3 series)

Input terminals of the FX3 series are wired and the "X0" terminal and the "0V" terminal are short-circuited. However, the input does not turn on.
Category : 

Answer

For the sink input, the "S/S" terminal and the "24V" terminal are needed to be short-circuited.
Product Name
FX3S, FX3G, FX3GC, FX3U, FX3UC
Product Category
Main unit, I/O Extension
Series
FX3S, FX3G, FX3GC, FX3U, FX3UC