• No : 22269
  • Release Date : 2018/08/30 13:48
  • Print

Deleting all programs and data from the memory

How can I delete all programs and data in memory in the MELSEC-F series?
Category : 

Answer

Data can be cleared from GX Developer or GX Works2.
[Online]→Select all [PLC memory], [Data device], and [Bit device.] on the Clear PLC memory window, and execute the clear operation.
Product Name
FX1S, FX1N, FX1NC, FX2N, FX2NC, FX3S, FX3G, FX3GC, FX3U, FX3UC
Product Category
Main unit, Engineering Software, GX Developper, GX Works2
Series
MELSEC-F series