• No : 22274
  • Release Date : 2018/08/30 13:48
  • Print

Multiple input COM terminals

Answer

All input COM terminals send the same signal because all the terminals are internally connected.
To turn on the input, the extension unit must be connected to the main unit.
Product Name
FX1S, FX1N, FX1NC, FX2N, FX2NC, FX3S, FX3G, FX3GC, FX3U, FX3UC
Product Category
Main unit, I/O Extension
Series
MELSEC-F series