• No : 22307
  • Release Date : 2018/08/30 13:55
  • Update : 2018/09/28 15:09
  • Print

Regarding I/O assignment on the module configuration diagram of GX Works3

Is it possible to check the I/O assignment of CPU or I/O extension modules on module configuration diagram of GX Works3?
Category : 

Answer

While the module configuration window is being displayed,
the I/O assignment can be checked by selecting the following options from the menu bar:
[Edit]→[XY Assignment Display]
Product Name
FX5U, FX5UC
Product Category
CPU Module, I/O Module, Engineering Software, GX Works3
Series
MELSEC iQ-F Series