- No : 22310
- Release Date : 2018/08/30 13:55
-
Print
Regarding the maximum number of high-speed counters which can be used
How many high-speed counters are available for the CPU module?
- Category :
-
Answer
The high-speed counter supports 1-phase 1-input, 1-phase 2-input, 2-phase 2-input.
The built-in counter in the CPU module can input up to 8ch.
However, in the case of 32 point type CPU module, the maximum response frequency differs depending on the channel.
- FX5U/FX5UC CPU module (32 points):
200kHz 6ch,10kHz 2ch Total 8ch
- FX5U CPU module (64/80 points)、FX5UC CPU module(64/96 points):
200kHz 8ch
- Product Name
- FX5U, FX5UC
- Product Category
- CPU Module, High-Speed Counter
- Series
- MELSEC iQ-F Series