• No : 22315
  • Release Date : 2018/08/30 13:55
  • Update : 2022/12/22 10:23
  • Print

Regarding the digital output of the built-in analog function

Is it possible to scale the digital output value with the built-in analog input?
Category : 

Answer

It is possible by setting the scaling function or shift function from the parameter settings.
Product Name
FX5U
Product Category
CPU Module, Analog Control
Series
FX5U