• No : 22318
  • Release Date : 2018/08/30 13:55
  • Update : 2023/07/03 11:50
  • Print

Regarding the system configuration of FX5-CCL-MS with FX5 CPU module

Answer

A total of two FX5-CCL-MS (CC-Link system master/intelligent device) can be connected: one as a master station and one as an intelligent device station.
Product Name
FX5-CCL-MS
Product Category
Network/Communication
Series
MELSEC iQ-F Series