- No : 22324
- Release Date : 2018/08/30 13:55
-
Print
Regarding the maximum number of connections for MODBUS communication
When MODBUS communication is used as master station, how many slave stations can be connected?
- Category :
-
Answer
32 stations can be connected when RS-485 port is used and only 1 station can be connected when RS-232 port is used.
- Product Name
- FX5U, FX5UC
- Product Category
- CPU Module, Network/Communication
- Series
- MELSEC iQ-F Series