- No : 22902
- Release Date : 2018/09/03 17:30
-
Print
Accessing an A series Ethernet interface module via a router using GX Developer
Is it possible to connect GX Developer to an A series Ethernet interface module via a router using the Ethernet adapter on the personal computer?
- Category :
-
Answer
For GX Developer, a connection via an A series Ethernet interface module allows communication only within the same segment. Via a router, it is impossible to access programmable controller CPU modules within other segments via an A series Ethernet interface module.
- Product Name
- Engineering Software
- Series
- Software Package (GPP function)