- No : 22912
- Release Date : 2018/09/03 17:30
-
Print
Writing LJ71C24 modules' parameters using GX Works2
When are the switch setting and the settings of "Various Control Specifications" for the LJ71C24 series intelligent function modules written by GX Works2?
- Category :
-
Answer
The switch setting is written when CPU module's parameters are written. The settings of "Various Control Specifications" are written when intelligent function module settings are written.
- Product Name
- Engineering Software
- Series
- Software Package (GPP function)