- No : 23577
- Release Date : 2018/09/14 15:09
-
Print
Error 2035
What is error 2035?
What should I do when it occurs?
- Category :
-
Answer
Error 2035 (Command frequency error) occurs when the servo amplifier detects a command frequency error.
(1) When the command is the permissible speed or higher. Check operation pattern.
(2) When the command is lower than the permissible speed.
• Take countermeasure against I/O signal noise
• Take countermeasure against servo system controller noise
Refer to relevant servo amplifier manuals for details.
- Product Name
- Motion controller
- Series
- MELSEC-Q