- No : 23650
 
      - Release Date : 2018/09/14 15:10
 
        - 
          
              Print
          
        
 
  
 
Clearing the alarm history
    
      How can I clear the alarm history?
    
  
    - Category : 
 
    - 
      
    
 
  
 
    Answer
  
    By either of following methods: (MR-J4)
 1. On MR Configurator2, select [Diagnosis] - [Alarm Display] - [Clear]. 
 2. Set alarm history clear of parameter to "0001". 
(Type A: PC18, type B: PC21) 
When alarm history clear is enabled, the alarm history is cleared at next power-on. 
After the alarm history is cleared, the setting is automatically disabled, "0000”. 
  
    
      
        - Product Name
 
          - AC Servos-MELSERVO
 
      
      
        - Series
 
          - MELSERVO-J4