• No : 24699
  • Release Date : 2019/02/27 08:58
  • Print

Latch (backup) areas in the data register (D) and extended register (R) of the FX3U/FX3UC series

Which areas in the data register (D) and extended register (R) of the FX3U/FX3UC series can be latched?
Category : 

Answer

D200 to D7999 and R0 to R32767 can be latched.
D200 to D511 can be set as non-latch areas in parameters.
For details on the parameter setting, refer to the following.

Section 2.7.9 (3 Setting devices) in the FX3S/FX3G/FX3GC/FX3U/FX3UC Series Programmable Controllers Programming Manual [Basic & Applied Instruction Edition] (Manual number: JY997D16601)
 
Product Name
FX3U, FX3UC
Product Category
Main unit, Engineering Software, GX Works2, GX Developer
Series
MELSEC-F series