• No : 24776
  • Release Date : 2019/02/27 15:35
  • Print

Models of the MELSEC-F series main units

What are the differences among the suffixes, such as ES, ESS, DS, and DSS, of models of the MELSEC-F series main units?
Category : 

Answer

"E" represents AC power supply and "D" represents DC power supply.
The alphabets following "E" and "D" represent output types.
"S" represents replay output, triac output, or transistor output (sink).
"SS" represents transistor output (source).
Product Name
FX1S, FX1N, FX1NC, FX3S, FX3G, FX3GC, FX2N, FX2NC, FX3U, FX3UC
Product Category
Main unit
Series
MELSEC-F series