• No : 24779
  • Release Date : 2019/02/27 15:58
  • Print

Scan time while operation of a programmable controller CPU is being monitored using GX Works2

While operation of a programmable controller CPU is being monitored using GX Works2, the scan time displayed differs from the expected scan time.
Category : 

Answer

Scan time displayed on GX Works2 is the maximum scan time of the monitor target programmable controller CPU.
To check current scan time, monitor the data in D8010.
Product Name
FX1S, FX1N, FX1NC, FX3S, FX3G, FX3GC, FX2N, FX2NC, FX3U, FX3UC
Product Category
Main unit, Engineering Software, GX Works2, GX Developer
Series
MELSEC-F series