• No : 24786
  • Release Date : 2019/02/28 09:06
  • Print

24+ terminal connection of an extension block

Where should I connect the 24+ terminal of an extension block to?
Category : 

Answer

For AC power supply type, connect the 24+ terminal of an extension block to the 24+ terminal of a main unit.
For DC power supply type, connect the 24+ terminal of an extension block to the 24V+ terminal of an external power supply.
For details, refer to the manual for each product used.
Product Name
FX1S, FX1N, FX1NC, FX3S, FX3G, FX3GC, FX2N, FX2NC, FX3U, FX3UC
Product Category
Main unit, I/O Extension
Series
MELSEC-F series