• No : 24789
  • Release Date : 2019/02/28 09:07
  • Print

Data that can be stored in a memory cassette (FX3U/FX3UC)

Is it possible to store the device memory data in a memory cassette for the FX3U/FX3UC series?
Category : 

Answer

The device memory data cannot be stored in a memory cassette.
In the FX3U/FX3UC series, a part of device memory data can be latched using a battery.
The device memory data can be written to or read from the built-in RAM of a programmable controller and stored as part of the project data using a programming tool such as GX Works2.

For details, refer to the following.
 Section 15.1 in the GX Works2 Version 1 Operating Manual (Common) (Manual number: SH-080779ENG)
  
Data, such as programs, parameters, comments, file register, symbolic information, and extended file register, can be stored in a memory cassette.

* For details on the latch range setting, refer to the following.
Section 2.7 in the FX3S/FX3G/FX3GC/FX3U/FX3UC Series Programmable Controllers Programming Manual [Basic & Applied Instruction Edition] (Manual number: JY997D16601)

Reference) The main units with Ver. 3.00 or later support symbolic information.
   Since the capacity of symbolic information is large, use of the FX3U-FLROM-1M which has the dedicated areas for storing symbolic information is recommended.
Product Name
FX3G-EEPROM-32L,FX3U-FLROM-16,FX3U-FLROM-64,FX3U-FLROM-64L,FX3U-FLROM-1M
Product Category
Accessories, Options
Series
FX3U, FX3UC