For the first input extension block connecting to a main unit, use the FX2NC-100BPCB power supply cable provided with the main unit, and supply power from a 24 V DC power supply. For the second or later input block, use the FX2NC-10BPCB1 power supply cable provided with the input extension block, and connect it to either upper or lower power supply connector of the input extension block previously connected.