• No : 24949
  • Release Date : 2019/04/18 14:29
  • Print

Maximum length of input wiring

What is the maximum length of input wiring?
Category : 

Answer

Although it depends on the operating environment, wiring within 20 m is generally recommended.
Product Name
MELSEC-F Series
Product Category
FX1S, FX1N, FX1NC, FX3G, FX3GC, FX2N, FX2NC, FX3U, FX3UC
Series
Main Unit