• No : 24956
  • Release Date : 2019/04/18 14:28
  • Print

Differences between the FX3UC-32MT-LT and the FX3UC-32MT-LT2

What are differences between the FX3UC-32MT-LT and the FX3UC-32MT-LT2?
Category : 

Answer

The built-in CC-Link/LT setting differs. 
For the FX3UC-32MT-LT, the built-in CC-Link/LT setting is performed with the DIP switch. For the FX3UC-32MT-LT2, the setting is performed using GX Developer.
Product Name
MELSEC-F Series
Product Category
FX3UC
Series
Main Unit, Network/Communication