FAQ
>
Controllers
>
Programmable Controllers MELSEC
>
MELSEC-F Series
>
Main Unit
>
Differences between the FX3UC-32MT-LT and the FX3UC-32MT-LT2
Back
No : 24956
Release Date : 2019/04/18 14:28
Print
Differences between the FX3UC-32MT-LT and the FX3UC-32MT-LT2
What are differences between the FX3UC-32MT-LT and the FX3UC-32MT-LT2?
Category :
FAQ
>
Controllers
>
Programmable Controllers MELSEC
>
MELSEC-F Series
FAQ
>
Controllers
>
Programmable Controllers MELSEC
>
MELSEC-F Series
>
Main Unit
FAQ
>
Controllers
>
Programmable Controllers MELSEC
>
MELSEC-F Series
>
Network/Communication
Answer
The built-in CC-Link/LT setting differs.
For the FX3UC-32MT-LT, the built-in CC-Link/LT setting is performed with the DIP switch. For the FX3UC-32MT-LT2, the setting is performed using GX Developer.
Product Name
MELSEC-F Series
Product Category
FX3UC
Series
Main Unit, Network/Communication