• No : 24988
  • Release Date : 2019/04/23 07:22
  • Print

Instruction execution complete flag

The instruction execution complete flag does not turn on.
Category : 

Answer

When a flag contact is not programmed directly under the instruction to be checked, the flag may be turned off depending on the execution status of another instruction which shares M8029. Refer to Section 6.5.2 Handling of general flags in the FX3S/FX3G/FX3GC/FX3U/FX3UC Series Programming Manual Basic & Applied Instruction Edition.
Product Name
MELSEC-F Series
Product Category
FX1S, FX1N, FX1NC, FX3G, FX3GC, FX2N, FX2NC, FX3U, FX3UC
Series
Main Unit