• No : 24998
  • Release Date : 2019/04/23 10:38
  • Print

Remote maintenance

How can I change programs used in a remote facility?
Category : 

Answer

Remote maintenance can be performed by writing a program to a memory cassette and sending the program or by using a personal computer (GX Developer). With a programmable controller that supports the memory cassette equipped with the loader function, data in the memory cassette can be easily written to the built-in memory of the programmable controller without a personal computer (GX Developer) at the destination.
Product Name
MELSEC-F Series
Product Category
FX1S, FX1N, FX1NC, FX3G, FX3GC,FX2N, FX2NC, FX3U, FX3UC
Series
Main Unit