For the Connected/Disconnected Module Detection of FX5-CCLGN-MS, the network configuration of the subsequent stages can not be automatically detected unless the network has been established between the FX5-CCLGN-MS operating as the master station with at least one local or remote station.
Use the above function after establishing communication between FX5-CCLGN-MS with one or more local or remote stations.