When the power is turned on, the FX5-CCLGN-MS performs parameter check processing, and if an error occurs, the CPU module is also notified of the error. Therefore, an error code is also generated on the CPU module side. Resolving the FX5-CCLGN-MS error also clears the CPU module error.