FAQ
>
Controllers
>
Programmable Controllers MELSEC
>
MELSEC iQ-F Series
>
Regarding number of input/output points when adding safety extension module
Back
No : 39314
Release Date : 2023/01/12 16:54
Print
Regarding number of input/output points when adding safety extension module
If the FX5-SF-MU4T5 is added, will the number of I/O points that can be added to the FX5 CPU module be affected?
Category :
FAQ
>
Controllers
>
Programmable Controllers MELSEC
>
MELSEC iQ-F Series
FAQ
>
Controllers
>
Programmable Controllers MELSEC
>
MELSEC iQ-F Series
>
CPU Module
FAQ
>
Controllers
>
Programmable Controllers MELSEC
>
MELSEC iQ-F Series
>
Safety Control
Answer
It will. It is treated the same as an intelligent module, so it occupies 8 I/O points. The safety input expansion module FX5-SF-8DI4 does not occupy the number of I/O points even when it is expanded.
Product Name
FX5-SF-MU4T5、FX5-SF-8DI4
Product Category
CPU Module, Safety Control
Series
MELSEC iQ-F Series