• No : 39340
  • Release Date : 2023/02/14 17:28
  • Print

Regarding the FX5S CPU Module Line-up

How many input and output point types does the FX5S CPU module have?
Category : 

Answer

The line-up of input and output points of the FX5S CPU module is as follows.
・30 points (Input: 16 points, Output: 14 points)
・40 points (Input: 24 points, Output: 16 points)
・60 points (Input: 36 points, Output: 24 points)
Product Name
FX5S
Product Category
CPU Module
Series
MELSEC iQ-F Series