FAQ
>
Controllers
>
Programmable Controllers MELSEC
>
MELSEC iQ-F Series
>
Regarding the number of FX5-4A-ADP connections
Back
No : 39348
Release Date : 2023/02/15 10:16
Print
Regarding the number of FX5-4A-ADP connections
How many FX5-4A-ADPs can be connected to an FX5 CPU module?
Category :
FAQ
>
Controllers
>
Programmable Controllers MELSEC
>
MELSEC iQ-F Series
FAQ
>
Controllers
>
Programmable Controllers MELSEC
>
MELSEC iQ-F Series
>
CPU Module
FAQ
>
Controllers
>
Programmable Controllers MELSEC
>
MELSEC iQ-F Series
>
Analog
Answer
Up to 4 FX5-4A-ADPs can be connected to an FX5U/FX5UC/FX5S CPU module.
To connect 3 or more FX5-4A-ADPs, the FX5-4A-ADP must have a serial number S/N: 224 **** or later.
Up to 2 FX5-4A-ADPs can be connected to the FX5UJ CPU module.
Product Name
FX5U, FX5UC, FX5UJ, FX5S
Product Category
CPU Module, Analog
Series
MELSEC iQ-F Series