• No : 39350
  • Release Date : 2023/01/12 17:09
  • Update : 2025/03/07 13:25
  • Print

Regarding input of Differential Driver Output Type

Does the FX5 CPU module's built-in high-speed counter function allow pulse input from a DC5V differential driver output type encoder?
Category : 

Answer

It does not. The built-in high-speed counter function of the FX5U/FX5UC CPU module does not support DC5V input. 

DC5V input can be achieved by adding BUS conversion module FX5-CNV-BUS(C) + FX5-2HC/ES.
*The FX5-2HC/ES can be added to the FX5U/FX5UC/FX5UJ CPU modules.

Product Name
FX5U,FX5UC,FX5UJ,FX5S,FX5-2HC/ES
Product Category
CPU Module, High-Speed Counter
Series
MELSEC iQ-F Series