• No : 39364
  • Release Date : 2023/02/15 13:05
  • Print

Regarding the parallel link function between CPU modules

Can I use the parallel link function between the FX5 and FX3 CPU modules?
Category : 

Answer

Parallel linking between FX5 and FX3 CPU modules is not available. The N:N Network function supports communication between the FX5 CPU module and the FX3 CPU module.
Product Name
FX5U, FX5UC, FX5UJ, FX5S
Product Category
CPU Module, Network/Communication
Series
MELSEC iQ-F Series