FAQ
>
Controllers
>
Programmable Controllers MELSEC
>
MELSEC iQ-F Series
>
Regarding sending emails
Back
No : 40035
Release Date : 2023/08/24 15:40
Update : 2023/08/25 11:34
Print
Regarding sending emails
Is it possible to send emails with the iQ-F series?
Category :
FAQ
>
Controllers
>
Programmable Controllers MELSEC
>
MELSEC iQ-F Series
FAQ
>
Controllers
>
Programmable Controllers MELSEC
>
MELSEC iQ-F Series
>
Network/Communication
Answer
Using the email function of FX5-ENET, it is possible to send mail via a mail server.
The email function is supported in the following versions.
・Hardware serial number: 234 **** or later
・Firmware version 1.200 or later
Product Name
FX5-ENET
Product Category
Network/Communication
Series
MELSEC iQ-F Series