• No : 40035
  • Release Date : 2023/08/24 15:40
  • Update : 2023/08/25 11:34
  • Print

Regarding sending emails

Is it possible to send emails with the iQ-F series?
Category : 

Answer

Using the email function of FX5-ENET, it is possible to send mail via a mail server.
The email function is supported in the following versions.
・Hardware serial number: 234 **** or later
・Firmware version 1.200 or later
Product Name
FX5-ENET
Product Category
Network/Communication
Series
MELSEC iQ-F Series