The file formats and file sizes that can be attached by the email function are as follows:
・Attachments: Up to one file
・File formats: Binary, ASCII, CSV
・File size: 32768 bytes
*The attached data must be generated by a program. Therefore, files (such as logging data) in the CPU module or SD memory card can not be attached.