• No : 40057
  • Release Date : 2023/08/25 10:21
  • Print

Regarding Email function Attachments

What are the file formats and file sizes that can be attached by the email function?
Category : 

Answer

The file formats and file sizes that can be attached by the email function are as follows:
・Attachments: Up to one file
・File formats: Binary, ASCII, CSV
・File size: 32768 bytes
*The attached data must be generated by a program. Therefore, files (such as logging data) in the CPU module or SD memory card can not be attached.
Product Name
FX5-ENET
Product Category
Network/Communication
Series
MELSEC iQ-F Series