The following points are different for the iQ-F series.
・Error History
If the FX5 CPU Module is turned off, the error history is cleared.
・Setting details of the CPU Module Logging Configuration Tool
DNS server settings are not supported.
・Directory
If the specified directory does not exist on the FTP server, no error occurs and the directory is created and the file is transferred.