• No : 44476
  • Release Date : 2024/07/02 19:06
  • Print

Regarding understanding the difference between "Batch Setting of PDO Mapping" and "PDO Mapping Setting".

What is the difference between setting up "Batch Setting of PDO Mapping" or "PDO Mapping Setting"?
Category : 

Answer

The batch setting of PDO mapping sets the default PDO mapping for all device stations that support PDO mapping.
*Note that in the batch setting of PDO mapping, the 1st mapping pattern which is not supported by FX5-CCLGN-MS is set.
The PDO mapping configuration sets the PDO mapping for each device station that supports PDO mapping.
 
See the manual below.
MELSEC iQ-F FX5 CC-Link IE TSN Master/Local Module User's Manual
Product Name
FX5-CCLGN-MS
Product Category
Network/Communication
Series
MELSEC iQ-F Series